AXIS#.DIR

Description

AXIS#.DIR changes the direction of the motor by changing the algebraic sign of the current command and position feedback value according to the figure below.

Note the following when using AXIS#.DIR:

  • You can only change the AXIS#.DIR command when the drive is disabled.
  • The drive status changes to "Axis not homed" as soon as the AXIS#.DIR parameter changes value (see AXIS#.MOTIONSTAT).
  • You must verify the settings of the hardware limit switches. If necessary, switch the positive and negative hardware limit switches by swapping the wires at the digital inputs.

 

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Read/Write

Units

N/A

Range

0 to 1
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
AXIS1.DIR

5000h

0fh

Unsigned8

-

-

Read/Write

No

AXIS2.DIR

5100h

0fh

Unsigned8

-

-

Read/Write

No

EtherNet/IP

Name

ID

Hex

Data Type

Access

Units

AXIS1.DIR

5006

138E

Unsigned8

Read/Write

-

AXIS2.DIR

70542

1138

Unsigned8

Read/Write

-

PROFINET

Parameter

PNU

Data Type

Access

Units

AXIS#.DIR

5006

Unsigned8

Read/Write

-